You are here: Getting Started > Manage a Project

Managing a Project

The New command in the File menu uses a wizard to help you to define the project.

The Open... command opens a window to let you navigate your system and retrieve previous projects.

The Save command saves your entire project.

The Save As... command allows you to save your project with a custom name and location.

The Close command prompts you to save first if some modifications have not been saved.

The Print... command allows you to create documentation containing editors' programs or diagrams.

For more details on the File menu, also refer to Menus and Toolbar Overview.

When editing your project, the KAS IDE has the following restrictions:

Use a Version Control System

To ensure integrity of your project files, you have to rely on tools to control versions.

Generally, such tools also have facilities for:

 

Print

Use the Reference Folder


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™